Cant connect to my device when running JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cant connect to my device when running JTAG

723件の閲覧回数
Nona
Contributor I

Hey, 

 

Im using JTAG - LPC4370 (LPC-Link Rev B) on my device.
my device is used as server and i connect to it on TCP port 5000

Only when im using the Debugger (through KEIL uvision4) - i cant connect to the device. 

I get "TCP connection timeout" 
i cant even PING to it. ("Destination host unreachable.")

Is there a setting that block the device ?

do you know what can be the reason ? 

Thanks.

0 件の賞賛
返信
1 返信

709件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Nona 

How about first try to directly use LPC-Link to connect your board with IDE, do not use TCP?

If still can not connect, how about check JTAG hardware:

https://community.nxp.com/thread/388998 

 

BR

Alice

0 件の賞賛
返信