Cannot wake up 11u68 with pin interrupt by GPIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot wake up 11u68 with pin interrupt by GPIO

2,380件の閲覧回数
leechen
Contributor III

I'm able to make my LPC11u68 into deep sleep mode, but i cannot wake it up. Can anyone help me?

 

The pin interrupt works if I don't put the MCU into Deep Sleep.  However, I cannot wake up the MCU if putting it to deep sleep mode by interrupting with GPIO.

#define GPIO_PININT_PIN               0     

#define GPIO_PININT_PORT              1

#define GPIO_PININT_INDEX             0

#define PININT_IRQ_HANDLER       PIN_INT0_IRQHandler     

#define PININT_NVIC_NAME         PIN_INT0_IRQn     

 

void PININT_IRQ_HANDLER(void)

{

     Chip_PININT_ClearIntStatus(LPC_PININT, PININTCH(GPIO_PININT_INDEX));

}

 

 

int main(void)

{

     CHIP_PMU_MCUPOWER_T crntPowerSetting;

 

     SystemCoreClockUpdate();

     Board_Init();

     SysTick_Config(SystemCoreClock / 10000 / 30);

 

     Chip_IOCON_PinMuxSet(LPC_IOCON, GPIO_PININT_PORT, GPIO_PININT_PIN,

               (IOCON_FUNC0 | IOCON_MODE_PULLUP | IOCON_CLKDIV(0) | IOCON_S_MODE(3)));

 

     Chip_GPIO_SetPinDIRInput(LPC_GPIO, GPIO_PININT_PORT, GPIO_PININT_PIN);

     Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_PINT);

     Chip_SYSCTL_SetPinInterrupt(GPIO_PININT_INDEX, GPIO_PININT_PORT, GPIO_PININT_PIN);

     Chip_PININT_ClearIntStatus(LPC_PININT, PININTCH(GPIO_PININT_INDEX));

     Chip_PININT_SetPinModeEdge(LPC_PININT, PININTCH(GPIO_PININT_INDEX));

     Chip_PININT_EnableIntLow(LPC_PININT, PININTCH(GPIO_PININT_INDEX));

     NVIC_ClearPendingIRQ(PININT_NVIC_NAME);

     NVIC_EnableIRQ(PININT_NVIC_NAME);

 

     Chip_SYSCTL_EnablePeriphWakeup(SYSCTL_WAKEUP_GPIOINT1);

     crntPowerSetting = PMU_MCU_DEEP_SLEEP;

 

     while (1) {

          ProcessPowerState(crntPowerSetting);

     }

     return 0;

}

2 返答(返信)

2,101件の閲覧回数
magicoe_niu
NXP Employee
NXP Employee

i intend use pin interrupt to wake-up MCU from power down modes.

Feel the pin interrupt can not wake up MCU from deep sleep and power down modes, after check your post content and the UM.

Only Group interrupt can help us wake up MCU from DSleep and Pdown modes.

Thank refer my codes as attached.

Thank you!

Thank you!

2,101件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  Lee Chen,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.

 

To provide the fastest possible support, I'd highly recommend you to refer to the periph_pinint demo in the LPCOpen library.

LPCOpen Software for LPC11XX|NXP 

TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
0 件の賞賛
返信