Cannot put LPC4320 into DFU mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot put LPC4320 into DFU mode

3,217 次查看
adityat
Contributor I

Hello,

        I am unable to put LPC4320 into DFU mode . The chip is working since the previous uploaded code is still executing on power on . The device doesn't show up on lsusb or dmesg either . How should I proceed to rectify this problem ?

Thanking You

Regards

标签 (2)
标记 (2)
0 项奖励
回复
3 回复数

3,003 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.
Yes, I don't think you actualy boot from the USB, I'd like to demonstrate the responding message after input the lsusb and dmesg command.
$ lsusb
Bus 002 Device 002: ID 8087:8000 Intel Corp. 
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 002: ID 8087:8008 Intel Corp. 
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 004 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 003 Device 003: ID 413c:2107 Dell Computer Corp. 
Bus 003 Device 002: ID 04ca:0061 Lite-On Technology Corp. 
Bus 003 Device 005: ID 1fc9:000c NXP Semiconductors 
Bus 003 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub



$ dmesg

[865677.700729] usb 3-10: new high-speed USB device number 6 using xhci_hcd
[865677.717570] usb 3-10: New USB device found, idVendor=1fc9, idProduct=000c
[865677.717579] usb 3-10: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[865677.717584] usb 3-10: Product: LPC
[865677.717588] usb 3-10: Manufacturer: NXP
[865677.717592] usb 3-10: SerialNumber: ABCD‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,003 次查看
neomissing
Contributor I

I have also encountered this problem, LPC onboard simulator can not DFUQQ截图20170420192438.png

0 项奖励
回复

3,003 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi neomissing,

Please refer to the reference manual to set the correct configuration to assure the MCU boot form the USB.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复