Cannot flash LPC55S69J MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot flash LPC55S69J MCU

2,846 Views
ay44
Contributor I

We are having issues flashing the LPC55S69J MCU. Flashing is performed via SWD.

This is the error message the IDE shows: Wire ACK Fault in DAP access

ay44_0-1666832523070.png

We've confirmed we have the right MCU orientation, correct voltages, etc. We are using the same setup that successfully flashes the LPC55S69-EVK.

Is there a particular pin configuration needed for the LPC55S69 MCU to flash? Anything missing from the setup detailed? 

 

** Setup **

Hardware platforms used:

- Custom designed board
- Breakout board with LPC55S69J MCU soldered on (Digikey PN: PA0096-ND)
- MCU-LINK board

 

Hardware notes:

MCU: LPC55S69JBD64K

SWDIO: pulled up via 100k; connected to pin 5 of MCU

SWCLK: pulled down via 100k; connected to pin 6 of MCU

 

VBAT_PMU pulled high 3V3

Reset line observed high; pulls low from programmer

All VDD pins externally connected to 3V3

All VSS pins externally connected to ground

USB1 (high speed) used

 

Setup information:

NXP Eval kit used: LPC55S69-EVK

NXP Programmer: MCU-LINK

 

PC/IDE info:

Product: MCUXpresso IDE

Version: MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13]

Operating system: Windows 10

VM: OpenJDK 64-Bit Server VM (64 bit)

 

NXP LPCXpresso55S69 Development Board: https://www.nxp.com/design/development-boards/lpcxpresso-boards/lpcxpresso55s69-development-board:LP...

 

NXP MCU-Link Debug Probe: https://www.nxp.com/design/microcontrollers-developer-resources/mcu-link-debug-probe:MCU-LINK

 

Log information generated the IDE:

MCUXpresso IDE RedlinkMulti Driver v11.6 (Jul 12 2022 16:58:24 - crt_emu_cm_redlink build 4)

Found chip XML file in C:/ (removed)

(  5) Remote configuration complete

Reconnected to existing LinkServer process.

Connecting to probe 1 core 0 (using server started externally) reports:

'Ee(42). Could not connect to core.'

Retrying...

Reconnected to existing LinkServer process.

Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.

Failed on connect: Ee(42). Could not connect to core.

No connection to chip's debug port

0 Kudos
Reply
2 Replies

2,763 Views
ay44
Contributor I

Hi Jun Zhang,

Thank you for the reply. I was able to get the MCU to flash. We provided VDD_PMU with 1.1V and flashing worked after this.

Our application does not use the internal DCDC converter. Could you confirm if the LCP55S69 MCU will function correctly if we do not use the built in DCDC converter and just supply VDD_PMU pin with 1.1V?

0 Kudos
Reply

2,821 Views
ZhangJennie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply