Cannot correctly determine clock rates for UART0 /SSP1 APB clocks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot correctly determine clock rates for UART0 /SSP1 APB clocks

902件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfgardiner on Wed Jan 07 09:40:05 MST 2015
Hi,

I am developing a customer project based on the LPC1837. Using the lpcopen functions, I cannot determine the clockrate of the APB clocks driving the UART0 or SSP1 peripherals:

I have tried:
//   uart0Rate      = Chip_Clock_GetRate(CLK_APB0_UART0);
   uart0Rate      = Chip_Clock_GetBaseClocktHz(CLK_BASE_UART0);
   ssp1Rate       = Chip_Clock_GetRate(CLK_APB2_SSP1);

The value return is always zero.

I have the following setup which derives a 48 MHz base clock from the USB0 PLL:
   Chip_Clock_SetDivider(CLK_IDIV_A, CLKIN_USBPLL, 2);
   Chip_Clock_SetDivider(CLK_IDIV_B, CLKIN_IDIVA, 5);
   Chip_Clock_SetDivider(CLK_IDIV_C, CLKIN_IDIVA, 5);

   Chip_Clock_SetBaseClock(CLK_BASE_UART0, CLKIN_IDIVB, true, false);  
   Chip_Clock_SetBaseClock(CLK_BASE_UART1, CLKIN_IDIVB, true, false);

   Chip_Clock_SetBaseClock(CLK_BASE_SSP1, CLKIN_IDIVC, true, false);

   Chip_Clock_SetBaseClock(CLK_BASE_OUT, CLKIN_IDIVB, true, false);


I have verified that this works with a scope so it seems purely be an lpcopen software issue. If I feed the output from DIVA, DIVB or DIVC to CLKOUT[0] I measure the expected clock rates.

Thanks,
Charles
ラベル(1)
0 件の賞賛
返信
0 返答(返信)