Cannot access memory after clock config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot access memory after clock config

1,578件の閲覧回数
anto
Contributor II

I have configured the card MCB1700 (LPC1768) with the following parameters of clock:
1) RTC oscillator
2) MSEL: 0x2254 (8788)
3) NSEL:0x0001 (1)
4) the PLL1 disabled
the objective is to operate the clock cpu to 12Mhz via an external quartz of 32KHz.
Unfortunately after this configuration are no longer able to reprogram the micro.
Cannot access memory (@ 0x00000000, Write, Acc Size: 4 bytes)
This is the message that appears every time I try to riprogrammaare micro.

Can you suggest a way to unlock the micro and it can be reprogrammed.

Thanks

0 件の賞賛
返信
1 返信

1,528件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Antonello Stella

I suggest you to try programing your micro through ISP, please refer to chapter 32 of the LPC176x/5x User Manual: https://www.nxp.com/docs/en/user-guide/UM10360.pdf

Let me know if this is helpful, if you have more specific questions do not hesitate to ask me.

 

Best regards,

Omar

0 件の賞賛
返信