Cannot access memory after clock config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot access memory after clock config

1,557 Views
anto
Contributor II

I have configured the card MCB1700 (LPC1768) with the following parameters of clock:
1) RTC oscillator
2) MSEL: 0x2254 (8788)
3) NSEL:0x0001 (1)
4) the PLL1 disabled
the objective is to operate the clock cpu to 12Mhz via an external quartz of 32KHz.
Unfortunately after this configuration are no longer able to reprogram the micro.
Cannot access memory (@ 0x00000000, Write, Acc Size: 4 bytes)
This is the message that appears every time I try to riprogrammaare micro.

Can you suggest a way to unlock the micro and it can be reprogrammed.

Thanks

0 Kudos
Reply
1 Reply

1,507 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Antonello Stella

I suggest you to try programing your micro through ISP, please refer to chapter 32 of the LPC176x/5x User Manual: https://www.nxp.com/docs/en/user-guide/UM10360.pdf

Let me know if this is helpful, if you have more specific questions do not hesitate to ask me.

 

Best regards,

Omar

0 Kudos
Reply