Can't setup adc with config tools. Sampled channels section shows all channels disabled.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't setup adc with config tools. Sampled channels section shows all channels disabled.

跳至解决方案
1,585 次查看
jaycrossbee
Contributor II

I am trying to continuously sample ADC0 CH1, and have set up using config tools from inside MCUXpresso. When I choose Sampled channels the channel number column always has disabled written at the end.

I suppose rather than continously sample, I would like to use the systemTick to trigger a single channel sample and conversion every 10 ms.

Can you please explain what I am doing wrong in the first paragraph and also how to use the systick to periodically sample instead?

The configTool screen of ADC setupThe configTool screen of ADC setupShowing the code before mainShowing the code before main

For the first paragraph, here is the autogenerated config info (with extra info) from peripherals.c 

/*Begin paste

/***********************************************************************************************************************
* ADC0 initialization code
**********************************************************************************************************************/
/* clang-format off */
/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
instance:
- name: 'ADC0'
- type: 'lpc_adc'
- mode: 'ADC'
- custom_name_enabled: 'false'
- type_id: 'lpc_adc_d74172b5bd0591c0d32a6c93c043a67f'
- functional_group: 'BOARD_InitPeripherals'
- peripheral: 'ADC0'
- config_sets:
- fsl_adc:
- doSelfCalibration: 'true'
- adcConfig:
- clockMode: 'kADC_ClockSynchronousMode'
- clockSourceFreq: 'BOARD_BootClockIRC12M'
- clockDividerNumber: '0'
- enableLowPowerMode: 'false'
- voltageRange: 'kADC_HighVoltageRange'
- thresholdConfig:
- ADC_SetThreshold0: 'false'
- thresholdSettingsPair0:
- lowValue: '0'
- highValue: '0'
- ADC_SetThreshold1: 'false'
- thresholdSettingsPair1:
- lowValue: '0'
- highValue: '0'
- enableSeqConfigurationA: 'true'
- adcConvSeqConfigA:
- enableHighPriority: 'true'
- adcConvSeqConfig:
- triggerMaskM: '0U'
- triggerPolarity: 'kADC_TriggerPolarityNegativeEdge'
- enableSyncBypass: 'false'
- enableSingleStep: 'false'
- interruptMode: 'kADC_InterruptForEachConversion'
- enableSeqConfigurationB: 'false'
- adcConvSeqConfigB:
- enableHighPriority: 'false'
- adcConvSeqConfig:
- triggerMaskM: '0U'
- triggerPolarity: 'kADC_TriggerPolarityNegativeEdge'
- enableSyncBypass: 'false'
- enableSingleStep: 'false'
- interruptMode: 'kADC_InterruptForEachConversion'
- channels:
- 0:
- channelName: ''
- channelNumber: 'CH.1'
- channelThresholdPair: 'thresholdPair0'
- thresholdInterruptMode: 'kADC_ThresholdInterruptDisabled'
- conversion_sequence: 'a'
- interrupt_sel: 'kADC_ConvSeqAInterruptEnable'
- enable_irq_seqA: 'true'
- adc_interrupt_seqA:
- IRQn: 'ADC0_SEQA_IRQn'
- enable_interrrupt: 'enabled'
- enable_priority: 'true'
- priority: '3'
- enable_custom_name: 'false'
- enable_irq_seqB: 'false'
- adc_interrupt_seqB:
- IRQn: 'ADC0_SEQB_IRQn'
- enable_interrrupt: 'enabled'
- enable_priority: 'false'
- priority: '0'
- enable_custom_name: 'false'
- enable_irq_thcmp: 'false'
- adc_interrupt_thcmp:
- IRQn: 'ADC0_THCMP_IRQn'
- enable_interrrupt: 'enabled'
- enable_priority: 'false'
- priority: '0'
- enable_custom_name: 'false'
- enable_irq_ovr: 'false'
- adc_interrupt_ovr:
- IRQn: 'ADC0_OVR_IRQn'
- enable_interrrupt: 'enabled'
- enable_priority: 'false'
- priority: '0'
- enable_custom_name: 'false'
* BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/
/* clang-format on */
const adc_config_t ADC0configStruct = {
.clockDividerNumber = 0UL,
.enableLowPowerMode = false,
.voltageRange = kADC_HighVoltageRange,
};
/* Conversion sequence A configuration structure */
const adc_conv_seq_config_t ADC0ConvSeqAConfigStruct = {
.channelMask = 2U,
.triggerMask = 0U,
.triggerPolarity = kADC_TriggerPolarityNegativeEdge,
.enableSyncBypass = false,
.enableSingleStep = false,
.interruptMode = kADC_InterruptForEachConversion
};

static void ADC0_init(void) {
/* Perform self calibration */
ADC_DoSelfCalibration(ADC0_PERIPHERAL, ADC0_CLK_FREQ);
/* Initialize ADC0 peripheral */
ADC_Init(ADC0_PERIPHERAL, &ADC0configStruct);
/* Configure priority for sequence A */
ADC_SetConvSeqAHighPriority(ADC0_PERIPHERAL);
/* Configure the conversion sequence A */
ADC_SetConvSeqAConfig(ADC0_PERIPHERAL, &ADC0ConvSeqAConfigStruct);
/* Enable the conversion sequence A */
ADC_EnableConvSeqA(ADC0_PERIPHERAL, true);
/* Enable interrupt from ADC */
ADC_EnableInterrupts(ADC0_PERIPHERAL, kADC_ConvSeqAInterruptEnable);
/* Configure threshold compare interrupt on channel 1 */
ADC_EnableThresholdCompareInterrupt(ADC0_PERIPHERAL, 1U, kADC_ThresholdInterruptDisabled);
/* Interrupt vector ADC0_SEQA_IRQn priority settings in the NVIC. */
NVIC_SetPriority(ADC0_ADC_SEQ_A_IRQN, ADC0_ADC_SEQ_A_IRQ_PRIORITY);
/* Enable interrupt ADC0_SEQA_IRQn request in the NVIC. */
EnableIRQ(ADC0_ADC_SEQ_A_IRQN);
}

End past*/

标签 (1)
0 项奖励
回复
1 解答
1,568 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

You can use BURST mode, there is lpc_adc_burst demo under SDK.

 

BR

Alice

在原帖中查看解决方案

2 回复数
1,569 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

You can use BURST mode, there is lpc_adc_burst demo under SDK.

 

BR

Alice

1,564 次查看
jaycrossbee
Contributor II
Thank you Alice, that is what I wanted. Can you recommend where I would see how to start a conversion from the sysTick handler?
0 项奖励
回复