Can't progrm or debug anymore SWD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't progrm or debug anymore SWD

1,679件の閲覧回数
xirxe
Contributor I

I have a board with SWD connecction, which works fine until I add a single line to the source

Chip_Clock_SetSystemPLLSource(SYSCTL_PLLCLKSRC_SYSOSC);

Now I'm not able to attach the GDB-Server ("CPU not connected") nor with my stand alone programming tool (J-Flash).

I tried it with different reset strategies and I can verify different signals on the reset line, but still the same, it's not possible to connect to the board.

Also, it's not a problem of a single board, I tried the same with  two more boards with the same result.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,511件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the below link:

ISP Reset over debug 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,511件の閲覧回数
vojtechhavlicek
Contributor III

Try to get into the ISP programming mode via pin 12 It should work (I think).

0 件の賞賛
返信