Can't able to generate clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't able to generate clock

1,693件の閲覧回数
faziya
Contributor I

Hi Everyone!

I am using LPC54S0JBD208 controller in my project as intial stage i have installed ExpressoIDE and later SDC

and after that i tried to select the development board of LPC54SO18 development board as there is no option to select the directcontroller later in project configuration i selected  LPC54S0JBD208 controller during this time IDe throw a warning ie., Board configuration files (such as pin-mux and clock-config) are not designed and might not work with the selected device. It's recommended to use Empty Board Files instead.

I selected emptyboardfiles this time it given another warning ie.,  Choosing empty board files may cause the absence of some defines (eg. BOARD_FLASH_SIZE). so i neglected that warning and created project later i opened clock configuration in IDE and tried to configure clock but it is always thowing an error 

are there any videos /document to generate clock for this controller if so please share for refering.

Thank you,

ANIL

0 件の賞賛
返信
2 返答(返信)

1,601件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @faziya 

Sorry to reply late, because there is issue with our network for that days, so missed your case, sorry.

If still have issue, please tell me, I will help you, thanks.

 

BR

Alice

0 件の賞賛
返信

1,490件の閲覧回数
koray692
Contributor II

Hello @Alice_Yang ,I have similar problem could you please help me ?

0 件の賞賛
返信