Can message filtering

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can message filtering

3,948 Views
andreaskneissl
Contributor II

I am confused with the description of the CAN messaeg filter in the LPC43xx manual. The cpu has 2 CAN interfaces. Every CAN interface has two message interface to filter the CAN bus for defined identifier. For each message interface I can define up to 32 identifier.

1) Does it mean, that I can define 64 identifier for CAN0 and 64 identifier for CAN1 or only 32 for CAN0 and 32 for CAN1?
2)   If I can scan only 32 identifier for each CAN-bus (the picture in the manual at page 1236 shows this) - why I need two message interfaces for each CAN bus?

3) If I want to change the identifier or to remove it from the filter list - how to do this?

4) Is there any code example available to show the using/modification of message filter?

5) Can I change the message filter during running CAN-bus or should I disable the CAN-interrupt during this process?

Labels (2)
0 Kudos
Reply
2 Replies

3,350 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andreas Kneissl,

   This question nearly the same as your anther question, please refer to my reply in your anther question at first:

https://community.nxp.com/thread/441359 

You can configure the can in the test mode, and enable the basic mode.

   Please modify the code like this:

CCAN_MSG_OBJ_T can_msg;

void CAN0_IRQHandler(void)
{
     CCAN_MSG_OBJ_T msg_buf;
     uint32_t can_int, can_stat, i;
     while ( (can_int = Chip_CCAN_GetIntID(LPC_C_CAN0)) != 0 ) {
          //if ((can_int & CCAN_INT_STATUS) ) 
                if ((CCAN_INT_STATUS == can_int) && (CCAN_STAT_RXOK & LPC_C_CAN0->STAT))
                {
                  //CCAN_MSG_OBJ_T can_msg;

                  can_msg.id = (uint32_t) (LPC_C_CAN0->IF[1].ARB1 | LPC_C_CAN0->IF[1].ARB2 << 16);

                  if (can_msg.id & (0x1 << 30)){
                     can_msg.id &= CCAN_MSG_ID_EXT_MASK;
                    }
                  else {
                     can_msg.id >>= 18;
                     can_msg.id &= CCAN_MSG_ID_STD_MASK;
                   }

                  can_msg.dlc = (uint8_t) (LPC_C_CAN0->IF[1].MCTRL & CCAN_IF_MCTRL_DLC_MSK);

                  *((uint16_t *)&can_msg.data[0]) = (uint16_t) (LPC_C_CAN0->IF[1].DA1 & 0x0000FFFF);
                  *((uint16_t *)&can_msg.data[2]) = (uint16_t) (LPC_C_CAN0->IF[1].DA2 & 0x0000FFFF);
                  *((uint16_t *)&can_msg.data[4]) = (uint16_t) (LPC_C_CAN0->IF[1].DB1 & 0x0000FFFF);
                  *((uint16_t *)&can_msg.data[6]) = (uint16_t) (LPC_C_CAN0->IF[1].DB2 & 0x0000FFFF);

                 
                  DEBUGOUT("can_msg ID :%x\r\n", can_msg.id);
                    DEBUGOUT("can_msg data :");
                    for (i = 0; i < can_msg.dlc; i++) {
                         DEBUGOUT("%x ", can_msg.data[i]);
                    }
                    DEBUGOUT("\r\nFeed back...\r\n");
                  Rx_Flag =1;
                  LPC_C_CAN0->STAT = LPC_C_CAN0->STAT & (~CCAN_STAT_RXOK);

                  return;
                }

     }
}
int main(void)
{
     CCAN_MSG_OBJ_T send_obj;
     SystemCoreClockUpdate();
     Board_Init();
     set_pinmux();
     DEBUGOUT(WelcomeMenu);
     /* Set CCAN peripheral clock under 100Mhz for working stable */
     Chip_Clock_SetBaseClock(CLK_BASE_APB3, CLKIN_IDIVC, true, false);
     Chip_CCAN_Init(LPC_C_CAN0);
        Chip_CCAN_EnableTestMode(LPC_C_CAN0);//jjadd
       // Chip_CCAN_ConfigTestMode(LPC_C_CAN0, ( CCAN_TEST_BASIC_MODE));//jjadd //CCAN_TEST_SILENT_MODE |
     Chip_CCAN_SetBitRate(LPC_C_CAN0, 500000);
     Chip_CCAN_EnableInt(LPC_C_CAN0, (CCAN_CTRL_IE | CCAN_CTRL_SIE | CCAN_CTRL_EIE));

     send_obj.id = CCAN_TX_MSG_ID;
     send_obj.dlc = 4;
     send_obj.data[0] = 'A';
     send_obj.data[1] = 'B';
     send_obj.data[2] = 'C';
     send_obj.data[3] = 'D';
     Chip_CCAN_Send(LPC_C_CAN0, CCAN_MSG_IF1, false, &send_obj);
     Chip_CCAN_ClearStatus(LPC_C_CAN0, CCAN_STAT_TXOK);


        Chip_CCAN_ConfigTestMode(LPC_C_CAN0, ( CCAN_TEST_BASIC_MODE));
        
     NVIC_EnableIRQ(C_CAN0_IRQn);

     while (1) {
        
        }
}

After modify like the above code, I can receive all the IDs.

The test result is:

pastedImage_1.png

Wish it helps you!

If you still have question, please let me know!

 


Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,350 Views
garyaltenberg
Contributor II

Hi Kerry,

I have the same question as the original in this thread. Your answer does not help. The question wasn't how to receive all messages but how does the receive filtering work. I don't want to receive from all nodes I just want to receive from a range of nodes. Is that possible? I would also be interested in all of the questions the original poster had.

1) Does it mean, that I can define 64 identifier for CAN0 and 64 identifier for CAN1 or only 32 for CAN0 and 32 for CAN1?
2)   If I can scan only 32 identifier for each CAN-bus (the picture in the manual at page 1236 shows this) - why I need two message interfaces for each CAN bus?

3) If I want to change the identifier or to remove it from the filter list - how to do this?

4) Is there any code example available to show the using/modification of message filter?

5) Can I change the message filter during running CAN-bus or should I disable the CAN-interrupt during this process?

Thank you,

Garyio

0 Kudos
Reply