Can i set the operating frequency of different for double core?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i set the operating frequency of different for double core?

872件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zhongjru on Wed Jan 07 02:37:51 MST 2015
I want to set different operating frequency for the 2 core,But I found 2 core using the same set of clock peripheral, not a separate set.In addition, enter low power mode, it is not a separate set of dormancy, such as M4F sleep and M0 running, can do it?
ラベル(1)
0 件の賞賛
返信
1 返信

789件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Wed Jan 07 13:20:36 MST 2015
Hi zhongjru,

When both cores are in active mode, they use the same clock source so they have to be operating at the same frequency. In terms of low power modes, Sleep mode can be used on one core and not the other. The other three low power modes, Deep-sleep, Power-down, and Deep Power-down, will force both cores into the low power mode since they shut down the chip.
0 件の賞賛
返信