Can SDA Pin Works if it connected to other GPIO pin which is also pulled up.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can SDA Pin Works if it connected to other GPIO pin which is also pulled up.

553件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by samson.p on Wed Jun 24 03:28:32 MST 2015
Hello Everyone,

Am working on  LPC1765 controller and am using Analog Sensor and I2C based Color sensor. Both sensors are connected one at a time.We designed in schematic like ADC pin(P0[23]) and SDA pin(P0[27])are joined together through switch  when we want to connect I2C based sensor.

My query is will my I2C sensor will work if i make that ADC pin which was connected to SDA pin as GPIO?

Kindly support me in this.

Regards,
Samson
ラベル(1)
0 件の賞賛
返信
0 返答(返信)