Can LPCXpresso tool program firmware generated by Keil uVision into internal flash via Keil uLink2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can LPCXpresso tool program firmware generated by Keil uVision into internal flash via Keil uLink2?

1,045 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by stanley76726 on Wed Mar 12 05:47:31 MST 2014
Hello all,

As titled, I tried but failed...  :(

For some reasons, I need to program the .axf file, pre-compiled by Keil uVision4,  to the internal flash of my LPC11C24/301.

The purpose of this is similar to mine.

So I connected uLink2 from the PC to the device, clicked the "Program Flash" button on LPCXpresso, and failed.

Error messages are described as follows:
    Flash driver "ProgramPage" timeout (300ms) PC: FFFFFFFE

Anyone has some experiences like this? Thanks!


标签 (1)
0 项奖励
回复
1 回复

1,025 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Wed Mar 12 14:55:17 MST 2014
Hi,

The Ulink2 with CMSIS DAP firmware will work with LPCXPresso IDE . Otherwise it will not work . It would be better if you  use LPCLink2 instead.

Thanks,

NXP Technical Support
0 项奖励
回复