Can I use SRAMX on the LPC55S69 for general data/array storage?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I use SRAMX on the LPC55S69 for general data/array storage?

2,195件の閲覧回数
davidcw
Contributor I

I've been using the LPC55S69 processor and despite a serious effort to bit-pack my memory usage, am running out of the 256KB of general purpose RAM. I have tried to use SRAMX for array storage, but am getting some intermittent faults.

I have read on other posts that I should be able to use SRAMX, and the user manuals for other LPC variants depict/describe the SRAMX on both the data/system-bus and code-bus, but that's not the way it's depicted in the block diagram on page 8 of the LPC55S6x user manual.

Question: Is there a special register/command I need to write to use SRAMX for data? Or, areas of SRAMX I should avoid using (even if I don't use the peripherals that would access those areas of SRAMX)?

As a contrived example, I would like to be able to execute code like the following:

uint8_t* array = (uint8_t*) (0x14000000);
array[0] = 128;
array[1] = 129;
array[2] = array[0]+array[1];
printf("value: %u", array[2]);

However, I have found that when I use SRAMX (in a similar way to how it is used in the example), I CAN read/write the array values, but I seem to be getting other intermittent bus and invalid state faults. I am NOT using SRAMX for any other peripheral (neither CASPER nor saving power down RAM state). I am running FreeRTOS with several interrupts and DMA.

Any insights would be helpful, thank you!

1 返信

2,180件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I copy the memory allocation of LPC55S69, pls use Non-secure address instead of secure address.

In detail, pls modify the first line to uint8_t* array = (uint8_t*) (0x04000000);

I am sure that the SRAMX can be used to save data and save/run code.

 

uint8_t* array = (uint8_t*) (0x04000000);
array[0] = 128;
array[1] = 129;
array[2] = array[0]+array[1];
printf("value: %u", array[2]);

 

xiangjun_rong_0-1632969983735.png

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信