Can I use NXP development tools under Linux?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I use NXP development tools under Linux?

813 次查看
Gvinity
Contributor I

Hello. 

I'm new to NXP and am considering the LPC11U6 for a design. However, I'm Linux-only: I don't have a Windows computer or workstation, and haven't used Microsoft since last century.

Can I use NXP development tools under Linux? Most grateful for any assistance.

...
0 项奖励
回复
1 回复

805 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @Gvinity ,

Thanks for considering our products. 

Can I use NXP development tools under Linux?

---> Yes. I recommend that you use MCUXpresso. It is compatible with Linux.
MCUXpresso IDE for NXP MCUs | Linux, Windows and MacOS | NXP Semiconductors | NXP Semiconductors

Celeste_Liu_0-1739874872064.pngCeleste_Liu_0-1739874872064.png

The SDK for LPC11U6 is in LPCOpen and it can be used in MCUXpresso. For the specific method, please refer to the link below.
MCUXpresso IDE - Using LPCOpen Examples | NXP Semiconductors

Hope it can help you.

BRs,

Celeste

 

----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复