Can I put the otp code into the flash programming algorithm?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I put the otp code into the flash programming algorithm?

1,647件の閲覧回数
cyc583723081
Contributor I

hi,

I have a brand new lpc4330 chip, but my experiment board doesn't control the external dial switch of the boot mode.Now I want to add opt in flash programming algorithm programming section, so that I can run in the flash programming otp fix for spifi program startup mode, there is no need for external dial the code switch my program can be started.I don't know if it's going to work.

0 件の賞賛
返信
2 返答(返信)

1,515件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Whether you want to program the OTP memory via the debugger.
If you do, I think this purpose can't get achieved.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,515件の閲覧回数
cyc583723081
Contributor I

hi,

In fact, I have added the otp programming to the flash burn algorithm, which has already implemented the programming of lpc4330 with the debugger, and no hardware pins are needed to choose the starting mode.Thank you very much.

0 件の賞賛
返信