Can I put the otp code into the flash programming algorithm?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I put the otp code into the flash programming algorithm?

1,665 次查看
cyc583723081
Contributor I

hi,

I have a brand new lpc4330 chip, but my experiment board doesn't control the external dial switch of the boot mode.Now I want to add opt in flash programming algorithm programming section, so that I can run in the flash programming otp fix for spifi program startup mode, there is no need for external dial the code switch my program can be started.I don't know if it's going to work.

0 项奖励
回复
2 回复数

1,533 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Whether you want to program the OTP memory via the debugger.
If you do, I think this purpose can't get achieved.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,533 次查看
cyc583723081
Contributor I

hi,

In fact, I have added the otp programming to the flash burn algorithm, which has already implemented the programming of lpc4330 with the debugger, and no hardware pins are needed to choose the starting mode.Thank you very much.

0 项奖励
回复