Can I get trace data out of the LPC2925?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I get trace data out of the LPC2925?

931 Views
edavis
Contributor I

I am using a LPC2925 processor. This processor has a JTAG standard connector. I notice

the processor has ETM/ETB within the processor. Can I get trace data out of the LPC2925? Does it

support SWO which is usually associated with Cortex whereas the LPC2925 is ARM9.

Bottom line, can I get trace data from the LPC2925?

0 Kudos
Reply
1 Reply

797 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Earl,

The LPC2925 device includes an ARM968E-S core with Embedded Trace Macrocell Interface. For additional details, you could take a look at the following links from ARM website:

http://infocenter.arm.com/help/topic/com.arm.doc.ddi0311d/Cihjggdi.html

http://infocenter.arm.com/help/topic/com.arm.doc.ddi0311d/Caccidaa.html


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply