Camera interface driver source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera interface driver source

2,597 Views
janmennen
Contributor II

I have a question about application software for the camera interface

AN12868SW - Camera Interface in LPC55S69

In the example only the library file LPC55S69_Camera_lib is included but no source code.

is there proprietary software used or why is the camera driver source not included?

I want to check if i can change the code for reading out a monochrome sensor 

Regards, Jan

0 Kudos
Reply
3 Replies

2,522 Views
janmennen
Contributor II

Hello Alice

I downloaded already but in the zip file there is only the already compiled liblpc55s69_camera_LIB.a library file.

I cannot find source code of the following functions called in  main.c

Camera_Init(); //camera engine initialization
Camera_Start(); //start camera engine

Regards, Jan

0 Kudos
Reply

2,522 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello jan, 

Yes, I also haven't find the source code of libs, 

If we want to request it, we need more information from you so that I can compose my internal request:

- your project name and scenarios

- the sufficient reason why you need it

- the chips ordered yearly.

- company name.

the market will evaluate and make decision if we have resource to arrange the test.

You can also send a secret massage to me about the above information.

Regards,

Alice

0 Kudos
Reply

2,522 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello jan mennen,

You can download the application code in the below thread:

https://www.nxp.com/docs/en/application-note-software/AN12868SW.zip 

It support MCUXpresso IDE and Keil MDK.

Regards,

Alice

0 Kudos
Reply