Calculate flash memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Calculate flash memory

Jump to solution
3,433 Views
Guy_mego
Contributor II

Hi,

I'm using LPC11U68 for my project. When I build my project on MCUXpresso IDE i see the usage of my flash memory. I know that is some MCUs there is given function or macro that gives the flash usage of flash memory. 
Is there a same for LPC11U68?

if not how can I calculate the usage of flash memory, in my code? I know the base address of my flash is:
0x0002 0000

Thanks.

Tags (1)
0 Kudos
Reply
1 Solution
3,425 Views
ErichStyger
Specialist I

There is the 'size' utility you can use to calculate the FLASH/RAM size, see

https://mcuoneclipse.com/2017/03/29/mcuxpresso-ide-s-record-intel-hex-and-binary-files/

how it is used in MCUXpresso IDE.

If you want to have more details: https://mcuoneclipse.com/2020/01/10/listing-code-and-data-size-for-all-files-with-the-gnu-size-utili...

Additionally, the MCUXpresso IDE includes a 'image info' view which gives you a lot of details too:

ErichStyger_0-1673976193101.pngErichStyger_0-1673976193101.png

 

I hope this helps,

Erich

View solution in original post

1 Reply
3,426 Views
ErichStyger
Specialist I

There is the 'size' utility you can use to calculate the FLASH/RAM size, see

https://mcuoneclipse.com/2017/03/29/mcuxpresso-ide-s-record-intel-hex-and-binary-files/

how it is used in MCUXpresso IDE.

If you want to have more details: https://mcuoneclipse.com/2020/01/10/listing-code-and-data-size-for-all-files-with-the-gnu-size-utili...

Additionally, the MCUXpresso IDE includes a 'image info' view which gives you a lot of details too:

ErichStyger_0-1673976193101.pngErichStyger_0-1673976193101.png

 

I hope this helps,

Erich