CPU Delay After Changing M4MEMMAP - LPC4337

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPU Delay After Changing M4MEMMAP - LPC4337

2,726件の閲覧回数
MikeBrennan
NXP Employee
NXP Employee

LPC4337

Have someone who is developing a boot loader which changes the CREG M4MEMMAP register to “shadow” an embedded application stored flash but is linked to 0x0.  He has this working but am noticing that the change in the memory map does not take effect immediately, in fact,  t seems he needs to insert at least 4 instructions before the next read from the “shadowed” memory region to make it work.

The documentation does not seem to mention such a delay.

Can you provide detail as to the exact delay (or suggested instruction sequence) following a change to this register?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,547件の閲覧回数
MikeBrennan
NXP Employee
NXP Employee

Any feedback on this?

Thanks,
Mike

0 件の賞賛
返信

2,547件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Michael,

What you mention may be a data synchronization issue. You can try using the isb and dsb intructions to flush the pipeline and ensure that all previous instructions are completed before executing new instructions, these are instructions of the ARM core which help to synchronize code execution and data accesses to avoid undesired behaviors.

You can find more information on this link:

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dai0321a/BIHEDAAF.html

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信