CORIDIUM LPC 1576

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CORIDIUM LPC 1576

1,241 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by HESPEK on Wed Jun 13 14:46:03 MST 2012
Have a coridium board ARM Cortex M3 LPC 1756
I am new to embeded design.

can anyone suggest a good Free Programming Environment compatible with ARM LPC 1756:
1. IDE
2. Compiler
3. Interface

Have some suggestion such as Codelite but not sure if compatiblee.

Thanks.
Labels (1)
0 Kudos
Reply
1 Reply

1,217 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfbsoftware on Mon Dec 10 04:49:45 MST 2012
Coridium's gcc-based C programming environment is 'no-frills' but it works very well. You can download it from the support pages on their website.

If you prefer to program in a language other than C, we have developed a complete IDE which uses the Oberon 2011 Programming Language (a modern version of Pascal / Modula-2) to generate native code for the LPC2000 and LPC13xx/LPC17xx micrcontrollers. We directly support both of Coridium's SuperPro Cortex-M3 boards as well as the LPCxpresso and Olimex boards:

http://www.astrobe.com/boards.htm
0 Kudos
Reply