COMPILATION ISSUE USING CDL LIBRARY

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

COMPILATION ISSUE USING CDL LIBRARY

985 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MOHAMMAD BIYABANI on Mon Jan 28 22:48:52 MST 2013
Hi,
I download the common driver library (CDL) from below URL
http://www.lpcware.com/content/nxpfile/lpc32x0-common-driver-library-cdl
and I have tried to set the environment for LPC3250 common driver library (CDL) from Windows XP by below procedure.
The procedure is:
1.In command prompt i set the environment where the generic is present for lpc32x0 by using command C:\nxpmcu\software>setenv generic_32x0 gnu 1
2. After that i went to below folder C:\nxpmcu\software\csps\lpc32xx\bsps\generic_32x0\startup\examples\Burners\nand_lb\kickstart

3.I make it by C:\nxpmcu\software\csps\lpc32xx\bsps\generic_32x0\startup\examples\Burners\nand_lb\kickstart>make
but it is showing errors like make <e=2>: The system cannot find the file specified. make:***[uart.0] Error 2

4.If i make it by C:\nxpmcu\software\csps\lpc32xx\bsps\generic_32x0\startup\examples\Burners\nand_sb\kickstart>make
then error is
make (e=2): The system cannot find the file specified.
make: *** [kickstart_nand_sb_burn.o] Error 2

5.For
C:\nxpmcu\software\csps\lpc32xx\bsps\generic_32x0\startup\examples\Burners\nor\norerase
the error is
make (e=2): The system cannot find the file specified.
make: *** [norerase.o] Error 2

HOW CAN I RECTIFY OR FIX IT?
标签 (1)
0 项奖励
回复
0 回复数