CMSIS, SPI driver is missing!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS, SPI driver is missing!

1,736件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mohammads on Mon Jul 14 21:52:30 MST 2014
Hello

I'm using Keil 5.10 professional, CMSIS 4.11. I want to use middlewares to connect to a web server, using LPC1788. But when I add ethernet driver to project, I get an error "require 2.01 CMSIS Driver:SPI","Install missing component!".
[img=982x642]http://community.arm.com/servlet/JiveServlet/downloadImage/2-20014-9004/11111111111111.png[/img]

SPI driver is in the list of API's In the CMSIS-Driver document, but it's not available for me!
I installed the latest version of Packs.
[img=1007x657]http://community.arm.com/servlet/JiveServlet/downloadImage/2-20014-9005/1222222222222222.png[/img]
where is the problem? I missed something or that's a software problem and I have to wait for new version?

[u]However, I want to use "DP83848, Ethernet PHY driver", not "KSZ8851SNL driver", but seems Its not possible!!![/u]

I have to write all of the TCP/IP and other things?



Thanks
ラベル(1)
0 件の賞賛
返信
1 返信

1,611件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jul 14 23:53:39 MST 2014

Quote: Mohammads
Hello

I'm using Keil 5.10 professional, CMSIS 4.11. I want to use middlewares to connect to a web server, using LPC1788. But when I add ethernet driver to project, I get an error "require 2.01 CMSIS Driver:SPI","Install missing component!".



I would suggest posting this on the Keil forums or contacting their customer support team. Links to both can be found at:

http://www.keil.com/support/

Regards,
LPCXpresso Support
0 件の賞賛
返信