CMSIS RTOS LPC18XX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS RTOS LPC18XX

2,160件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by manoS on Fri Apr 03 04:57:42 MST 2015
Hello,

I am working on LPC 18XX .
I am using CMSIS - CORE standard peripheral library for the project.
We need to use RTS for our project. Being new to Cortex -M3 can anyone clarify the following:

1. Do I need to use CMSIS-RTOS seperately along with CMSIS - CORE standard peripheral library?

2. Is CMSIS - RTOS library package available for RTX or Free RTOS?

3. I had read in an article that CMSIS pack ver 3 and above have support for CMSIS RTOS library. So , it it that we need to use both CORE standard peripheral library and CMSIS - RTOS library of same version? Because  CMSIS - CORE standard peripheral library for LPC18xx is of ver 2.


Looking forward for reply..
ラベル(1)
0 件の賞賛
返信
1 返信

2,061件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Fri Apr 03 10:46:24 MST 2015
Hi SonamK,

Do you have to use the CMSIS - CORE standard peripheral library on the LPC18xx? We have our own RTOS example in our LPCOpen software platform (which consists of a bunch of software examples to help jump-start developers new to the platform). If you are interested, feel free to check it out here:

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc18xx-packages-0

Also, we have a FreeRTOS page on using it with our microcontrollers which might also be of use:

http://www.lpcware.com/content/project/freertos-nxp-m0-m3-and-m4-mcus
0 件の賞賛
返信