CMSIS Link not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS Link not working

1,204件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mvkakati on Thu May 16 22:59:46 MST 2013

Hi,


 The CMSIS link


<ul>
<li class="zip"><a href="http://ics.nxp.com/support/lpcxpresso/zip/CMSISv2p00_LPC11xx.zip">CMSIS Library for LPC11xx</a> V2 (Jun 2, 2011) <img class="new" src="http://ics.nxp.com/images/pd-new.gif" border="0" alt="" /></li>
</ul>

at http://www.lpcware.com/content/project/nxp-peripherals/usb-nxp-microcontrollers/lpcxpresso-support is not working. Could you please direct me to the correct link.


 


Thanks,


Milind

ラベル(1)
0 件の賞賛
返信
1 返信

1,190件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Fri May 17 09:21:39 MST 2013

Miland
Thank you for bringing this to our attention.
The link should now be functional.


-paul

0 件の賞賛
返信