CMSIS FCLKSEL10 LPC54018

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS FCLKSEL10 LPC54018

ソリューションへジャンプ
2,449件の閲覧回数
danielgull
Contributor IV
Hi
In the SDK 2.7.0 for LPC54018 I have found this SYSCON_Type struct rather odd. The SPI10 with its FCLKSEL is defined separately from other SPI interface FCLKSEL. What is the reason? Can this be changed in the next SDK?
SDK_2.7.0_LPCXpresso54018\devices\LPC54018\LPC54018.h
Status Quo
typedef struct {
  ....
  __IO uint32_t FCLKSEL[10];
  __IO uint32_t FCLKSEL10;
  ....
} SYSCON_Type;
Proposal for change
typedef struct {
  ....
  __IO uint32_t FCLKSEL[11];
  ....
} SYSCON_Type;
Many thanks
Dani
ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,369件の閲覧回数
danielgull
Contributor IV

Hi XiangJun

Good point - that explains whay this register has a different name. I think it is best to keep the situation as is, because otherwise you could end up by setting the register the same as the others which will end up in a wrong configuration. The registers are not the same!

Suggestion:

Don't change anything and keep things the way they are.

Thank you for your valuable input and making me aware of this.

Dani

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,369件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Daniel,

Thank you for your pointing out the drawback of the SYSCON_Type structure. As you know that the UM11060.pdf defines two Table:

Table 121. Flexcomm Interface clock source select registers (FCLKSEL0-9, main syscon: offsets 0x2B0 through
2D4) bit description

Table 122. Flexcomm Interface clock source select registers (FCLKSEL10, main syscon: offset 2D8) bit description

Obviously, the address of FCLKSEL0-9 and FCLKSEL10 are continuous, but the engineers do not compute the address, so they define the  FCLKSEL10 independently as the UM.  But It does not take effect on the function and performance of the code.

Anyway, I will tell the firmware team of the question.

BR

XiangJun Rong

0 件の賞賛
返信
2,370件の閲覧回数
danielgull
Contributor IV

Hi XiangJun

Good point - that explains whay this register has a different name. I think it is best to keep the situation as is, because otherwise you could end up by setting the register the same as the others which will end up in a wrong configuration. The registers are not the same!

Suggestion:

Don't change anything and keep things the way they are.

Thank you for your valuable input and making me aware of this.

Dani

0 件の賞賛
返信