CLEV6630B with LPC1769 I/O Port Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLEV6630B with LPC1769 I/O Port Configuration

843 Views
N-K
Contributor I

I am working with the CLEV6630B NFC development kit and looking for guidance in updating the NfcrdlibEx1_DiscoveryLoop_mcux example program. For my application, I need to provide a logic high output when the tag is read successfully. It should be as simple as setting one of the dedicated test pins (P0.6-P0.9) to a logic 1, however, I am having trouble tracking down the location of the I/O configuration in the example project. I am relatively new to ARM based controllers and the NXP environment, so any guidance or advice is greatly appreciated. I am using the MCUXpresso IDE for development.

Labels (1)
0 Kudos
Reply
1 Reply

793 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @N-K 

You can refer to the demo "blinky". It includes how to config gpio high or low.

For LPC1769, recommend use LPCopen driver. About how to import project and use, I take a video for you. Please see my attachment.  Hope it helps. You can contact me if have any issue with it.

 

Best Regards,

Alice

0 Kudos
Reply