CCAN with ROM functions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCAN with ROM functions

1,239 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ipapp on Fri Nov 14 12:36:47 MST 2014
Hi,

Is there an example for the LPC43xx that uses the CCAN on-chip driver functions like there are examples for the LPC11xx(ie. this and this)? Or at least some documentation that explains how to implement it. There doesn't seem to be much information about this.

Thanks.
Labels (1)
0 Kudos
Reply
1 Reply

1,209 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Nov 14 13:36:45 MST 2014

Quote: ipapp
...for the LPC43xx that uses the CCAN on-chip driver...



:quest:

There's no CAN ROM API  :((

Chips with CAN ROM API are LPC11Cxx or LPC15xx...
0 Kudos
Reply