CCAN in LPC11C24

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCAN in LPC11C24

1,871 Views
ouseppachancr
Contributor I

data sheet of LPC11C24 says that it is  transceiver and have CANH and CANL lines.by giving proper termination also i didnt got any data in the bus.can anybody help me to sort out this problem....?

Labels (2)
0 Kudos
Reply
3 Replies

1,754 Views
ouseppachancr
Contributor I

and where is the example...?

0 Kudos
Reply

1,754 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ouseppachan Raphael,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to run periph_ccan_rom for testing, this example comes from the LPCOpen library and it shows how to use CCAN on-chip driver to send and receive a simple CAN frame.
Note: connect the CCAN_L and CCAN_H signal from the LPC11C24to a CAN-BUS Analyzer.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply