CCAN in LPC11C24

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CCAN in LPC11C24

2,744件の閲覧回数
ouseppachancr
Contributor I

data sheet of LPC11C24 says that it is  transceiver and have CANH and CANL lines.by giving proper termination also i didnt got any data in the bus.can anybody help me to sort out this problem....?

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,627件の閲覧回数
ouseppachancr
Contributor I

and where is the example...?

0 件の賞賛
返信

2,627件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ouseppachan Raphael,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to run periph_ccan_rom for testing, this example comes from the LPCOpen library and it shows how to use CCAN on-chip driver to send and receive a simple CAN frame.
Note: connect the CCAN_L and CCAN_H signal from the LPC11C24to a CAN-BUS Analyzer.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信