CANopen LPCXpresso55S16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CANopen LPCXpresso55S16

2,787件の閲覧回数
ahmed007
Contributor II

Hello, 

Are there any practical instances where CANopen FD is utilized in real-world applications, apart from the standard SDK examples for LPCXpresso55S16? 

Best regards,

Ahmed.

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,764件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ahmed007 

We only provide examples that can show the basic usage of every module of device, customer develop their own application based on it or just a reference. 

 

BR

Alice

0 件の賞賛
返信

2,742件の閲覧回数
ahmed007
Contributor II

Dear @Alice_Yang ,

 

I appreciate your response. I am currently encountering an issue with the connection between the LPCXpresso55S16 and Raspberry Pi 4 using CANopen.

When the two boards are not connected, the LPCXpresso displays the following frames:

ahmed007_0-1688977852436.png

This indicates that the CANopen example is functioning on the board. On the other hand, the Raspberry Pi shows these frames:

ahmed007_2-1688978067145.png

This suggests that CANopen is also working properly on the Raspberry Pi. However, when we connect both boards together, we observe the following frames:

ahmed007_3-1688978152642.png

At this point, the LPCXpresso frames show the ESI flag (Error State Indicator), which prevents the LPCXpresso from entering the operational mode and consequently disrupts communication between the two boards.

Do you have any suggestions or solutions for this issue?

 

Thank you for your assistance.

 

Best regards,

Ahmed 

0 件の賞賛
返信

2,726件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ahmed007 

How about check hardware connection?

 

BR

Alice

0 件の賞賛
返信

2,718件の閲覧回数
ahmed007
Contributor II

Hello @Alice_Yang ,

 

Also, one thing to mention, the Raspberry Pi uses a 500000 CAN  Bitrate and 2000000 CAN BRS_Bitrate while the LPCXpresso uses 500000 for both bitrates. 

I tried to change the Raspberry PI CAN_BRS_Bitrate to 500000 but I lose communication with it that's why I kept them as they were defined.

 

best regards,

Ahmed.

 

 

0 件の賞賛
返信

2,722件の閲覧回数
ahmed007
Contributor II

Hello @Alice_Yang ,

 

Thank you for your reply, Do you mean terminal resistors?

Best regards,

Ahmed Bouzid.

0 件の賞賛
返信