CANFD receive error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CANFD receive error

1,643件の閲覧回数
黎明孟
Contributor II

LPC54618 CANFD receive error:

The OM13094UL board used for CANFD and 500k/5M Baudrate used for communication;

It seems OK when only transmit out the data, the VehSpy used to monitor the CANFD frame;

 

But when use VehSpy to send the data to the board, the bus error occured;

As follow:

 

 

 

 

 

 

and when the bit rate switch disable, seems normal with VehSpy sending;

ラベル(1)
0 件の賞賛
返信
1 返信

1,538件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

This is a duplicated thread of: https://community.nxp.com/thread/503213 

0 件の賞賛
返信