CAN configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN configuration

1,442件の閲覧回数
minglunsheng
Contributor I

Hi

We are using the CAN interface on the LPC54608. We also use the fsl_can.c/h driver provided with the MCUXpresso SDK 2.5.0. The fsl_mcan.c function MCAN_SetMsgRAMBase(),MCAN_SetRxFifo0Config(),MCAN_SetTxBufferConfig().

I want to know how much memory MsgRAM will be allocated. And rxFifo0.elementSize ?  txBuffer.dedicatedSize?

Do you have  CAN configuration relevant instructions?

thanks    

alun

ラベル(1)
0 件の賞賛
返信
1 返信

1,380件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello minglun sheng ,

There is CAN demo under SDK package, you can refer it:

\SDK_2.6.0_LPCXpresso54608\boards\lpcxpresso54608\driver_examples\mcan

And recommend you use the latest version SDK v2.6, download from:

https://mcuxpresso.nxp.com/en/builder    

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信