CAN based project using lpc1769 and LPCOpen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN based project using lpc1769 and LPCOpen

1,399件の閲覧回数
aniketsgajare
Contributor I

I am trying to implement a simple project where I send a message from node 1 to node 2 using CAN. Both the nodes are lpc1769 boards. I suppose there are some issues with the code. As I am a beginner, I request you to provide any reference codes I can look into(polling implementation will be more helpful).

Thanking you in advance.

ラベル(3)
0 件の賞賛
返信
1 返信

1,330件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Aniket Gajare,

I recommend you refer to the "periph_can" demo under LPCOpen, there is a readme.txt ,

introduce how to use and config board in detail, please download it at :

LPCOpen Software for LPC17XX|NXP 

pastedImage_3.png

pastedImage_2.png

If have any question when using , please contact us without any hesitate.

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信