CAN ROM Driver about LPC15xx series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN ROM Driver about LPC15xx series

859件の閲覧回数
mountain777
Contributor I

 

Hi,

I have a question about CAN in the LPC15xx series.

I use the ROM Driver Interface to create a send and receive program and check the operation.

There is only one CAN interrupt in NVIC.

Therefore, I understand that CAN interrupts are shared for transmission and reception.

 

Is there a way to handle when CAN transmission and reception overlap?

I am worried that one of the communications will fail when the send and receive overlap.

 

Best regards

mountain777

0 件の賞賛
返信
0 返答(返信)