CAN- Automatic retransmission

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN- Automatic retransmission

1,127件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by akshimmu on Mon Apr 18 23:02:57 MST 2016
I have written the CAN driver for LPC1778 CAN module using Keil IDE as follows:

if(can12->SR & (1<<2) && (!bMsgSent))/*tx is free & msg not sent*/
{
can12->TFI1 = MsgBuf_TX.Frame; 
can12->TID1 = MsgBuf_TX.MsgID;
can12->TDA1 = MsgBuf_TX.DataA;
can12->TDB1 = MsgBuf_TX.DataB;
can12->CMR = m_bCAN_mode;
bMsgSent=1;
}

                delay_ms(100); //100 ms delay

if((can12->SR & (1<<3)) && bMsgSent) /*transmission complete*/
{
bReturn_val=1;
}


I have no other nodes on the bus and am using the simulator provided by keil. As per CAN Specs,a message is treated as successfully transmitted only after it has been acknowledged by any other node. But my doubt is, how does Bit 3 in GSR(Transmission complete) get set(bReturn_val=1) if no other nodes have acknowledged the transmitted message?
Is there something im missing?
The CAN is in normal mode.
ラベル(1)
0 件の賞賛
返信
1 返信

1,044件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信