Burst mode using PWM in LPC1788

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Burst mode using PWM in LPC1788

790件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by anuj.tanksali on Wed Feb 24 02:44:21 MST 2016
Hi.


I wanted to use burst mode for PWM channel1 in LPC1788
burst mode indicates. i want to given fixed no of pulses to PWM
Once i start the PWM the PWM should stop automatically after the no of pulses are over.
By stop automatically i mean in should not write any code to stop the PWM.
The PWM engine in LPC1788 should stop the PWM automatically after the user specified pulses are complete.
Can this be achieved using PWM channel1 in LPC1788

Thanks and Regards,

Anuj

ラベル(1)
0 件の賞賛
返信
0 返答(返信)