Burst mode using PWM in LPC1788

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Burst mode using PWM in LPC1788

780 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by anuj.tanksali on Wed Feb 24 02:44:21 MST 2016
Hi.


I wanted to use burst mode for PWM channel1 in LPC1788
burst mode indicates. i want to given fixed no of pulses to PWM
Once i start the PWM the PWM should stop automatically after the no of pulses are over.
By stop automatically i mean in should not write any code to stop the PWM.
The PWM engine in LPC1788 should stop the PWM automatically after the user specified pulses are complete.
Can this be achieved using PWM channel1 in LPC1788

Thanks and Regards,

Anuj

Labels (1)
0 Kudos
Reply
0 Replies