Build Issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Build Issues

1,217 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jeffbelz on Sun Mar 24 15:40:35 MST 2013
---Could not open file C:\Users\JBelz\Desktop\nxpUSBlib v0.98b\libraries\CDL\keil_output\CDL_LPC17xx.lib: No such file or directory

This is the Error when I compile.

Using:
uVision 4.70
nxpUSBlib 0.98b


When I use nxpUSBlib 0.97 i get this error
---Could not open file C:\Users\JBelz\Desktop\nxpUSBlib v0.97\libraries\BSP\keil_output\BSP_MCB1700.lib: No such file or directory

Seems that the packages are not complete.  I'm I correct, and how can I get the USB libraries working?
Is there an updated readme.txt, this has incorrect statements in them. Prob written for an older uVision.

Is there a place to download the .libs?
标签 (1)
0 项奖励
回复
1 回复

1,203 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jeffbelz on Mon Mar 25 06:43:48 MST 2013
never mind.  I figured it out.  I have to build the batch first.  I'm such a newb
0 项奖励
回复