Build Fails for FreeRTOS Demo on LPC1769 using LPCXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build Fails for FreeRTOS Demo on LPC1769 using LPCXpresso

1,295 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bubbzilla123 on Wed May 28 16:33:43 MST 2014
I'm trying to get the LPCXpresso LPC1768/LPC1769 FreeRTOS demo running on a LPCXpresso LPC1769 board with an LPC-Link attached. I've downloaded and activated the LPCXpresso IDE v7.2.0 using Windows 7 64-bit and followed the application instructions provided with the demo. I've successfully imported the demo which include three projects (CMSISv1p30_LPC17xx, FreeRTOS_Library, and SimpleDemo). FreeRTOS_Library builds successfully but the other two give errors:

CMSISv1p30_LPC17xx gives:
make: *** [src/core_cm3.o] Error 1
registers may not be the same -- `strexh r0,r0,[r1]'
registers may not be the same -- `strexb r0,r0,[r1]'


SimpleDemo gives:
cannot find -lCMSISv1p30_LPC17xx
make: *** [SimpleDemo.axf] Error 1


Any advice would be greatly appreciate.
Labels (1)
0 Kudos
Reply
1 Reply

1,232 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed May 28 17:02:47 MST 2014
See: http://www.lpcware.com/content/forum/cmsisv1p30lpc13xx-cannot-be-build-lpcxpresso-ide-ver7
0 Kudos
Reply