Bug-fix for Hitex LPC4357 kit to make RMII autoconfigure correctly

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bug-fix for Hitex LPC4357 kit to make RMII autoconfigure correctly

816 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rgledhill on Fri May 17 08:07:30 MST 2013

Hi,


There is a mistake on the Hitex LPC4357 kit where resistor R96 is 10k and needs to be 2k2.  This means that the auto-configure mode on the Ethernet PHY always defaults to MII mode, even if jumper JP5 is closed.


You can either change this resistor, or you can change your start-up code to force the PHY into RMII mode (if you want to use RMII mode!).  If you're using the Keil RTX TCPnet libraries, for instance, change ETH_LPC43xx.c:


:


:


            /* Configure the PHY device */
<strong>#if !_MII_ &amp;&amp; defined(HITEX_BOARD)</strong>
<strong>            write_PHY(PHY_REG_RBR, 0x20);   /* RMII mode - fix for Hitex LPC4357 board with inadequate config pull-up R96 */</strong>
<strong>#endif</strong>
#if defined(_10MBIT_)
:


:


 


This will be fixed in future revisions of the board; MII mode is unaffected.


Richard


Hitex UK Ltd

标签 (1)
0 项奖励
回复
0 回复数