Bug Report: iocon_13xx.h

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bug Report: iocon_13xx.h

1,295件の閲覧回数
janblumenkamp
Contributor I

Line 157/158:

#define IOCON_INV_EN            (0x1 << 6)/*!< Enables invert function on input */
#define IOCON_RESERVED_BIT_6    (0x1 << 6)/*!< Reserved, must be set. */

Bit 6 is responsible for inverting the pin! I just spent 6 hours tracking down why my UART is not working just because I set this bit... Not cool!

0 件の賞賛
返信
1 返信

1,205件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Jan,

Thanks for your sharing, and I will check later.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信