Brownout detection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Brownout detection

1,923 次查看
Pranavmv012
Contributor I

Hello, 

I am looking for brown out detection examples for LPC 1758 mcu, it is not clear how this should be enabled and how the interrupt is triggered. 

Is there any standard library for this. Please provide a coding example. 

Thanks in advance. 

 

0 项奖励
回复
2 回复数

1,876 次查看
Pranavmv012
Contributor I

Is it possible to set the voltage level at which the interrupt can be triggered. I could get the interrupt if the power goes below 2.3V now. 

 

0 项奖励
回复

1,909 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @Pranavmv012 

On User Manual UM10360 Chapter 3.5 Brown-out Detection. you will find information of how is enabled and triggered. I'll look for a example code.

Let me know if you have another question.

Best Regards, Miguel.

0 项奖励
回复