Brownout detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Brownout detection

1,899 Views
Pranavmv012
Contributor I

Hello, 

I am looking for brown out detection examples for LPC 1758 mcu, it is not clear how this should be enabled and how the interrupt is triggered. 

Is there any standard library for this. Please provide a coding example. 

Thanks in advance. 

 

0 Kudos
Reply
2 Replies

1,852 Views
Pranavmv012
Contributor I

Is it possible to set the voltage level at which the interrupt can be triggered. I could get the interrupt if the power goes below 2.3V now. 

 

0 Kudos
Reply

1,885 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @Pranavmv012 

On User Manual UM10360 Chapter 3.5 Brown-out Detection. you will find information of how is enabled and triggered. I'll look for a example code.

Let me know if you have another question.

Best Regards, Miguel.

0 Kudos
Reply