Brown out BOD voltage levels LPC433x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Brown out BOD voltage levels LPC433x

1,482件の閲覧回数
radomirkozub-re
NXP Employee
NXP Employee

Hello,

 

can somebody help me where to find voltage levels of BOD, both interrupt and reset.

 

User manual implicates that there are four levels of BOD voltage threshold, Level 0 to Level 3

 

 

 

however in data sheet there is are only two levels Level 2 and Level 3  mentioned.

 

 

Any idea?

 

Many thanks

 

Radomir

ラベル(1)
0 件の賞賛
返信
1 返信

1,335件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Radomir,

I beleive those levels were left out of that datasheet because the reset assertion points are quite far from the minimum operating VDD voltage. But you can still use the values from the LPC4350/30/20/10 datasheet as reference:

https://www.nxp.com/docs/en/data-sheet/LPC435X_3X_2X_1X.pdf 

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信