Brown Out detection Levels in LPC11U67

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Brown Out detection Levels in LPC11U67

1,620 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattiad on Fri Nov 21 08:14:12 MST 2014
Dears,

I want to use brown out detection in my microprocessor. In the user manual only levels are indicated, but I can't find which voltage ratio (compared to Vdd) corresponds to every level.
For example, with a voltage supply of 3.3V and a BOD level 3, which is the voltage level?

Best Regards,

Mattia
标签 (1)
0 项奖励
回复
3 回复数

1,422 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Nov 21 10:23:56 MST 2014

Quote: mattiad
Is it possible to know where you found it?



UM10462 downloaded from NXP.com after 'LPC11U67' search  :)
0 项奖励
回复

1,422 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattiad on Fri Nov 21 09:51:26 MST 2014
Thank you very much for your fast and clear answer!

Is it possible to know where you found it?

Best Regards,

Mattia
0 项奖励
回复

1,422 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Nov 21 09:07:26 MST 2014
:quest:

UM10462, Table 36:

Quote:

1:0 BODRSTLEV BOD reset level 0
0x0 [color=#f00]Level 0[/color]: The reset assertion threshold voltage is 1.46 V; the
reset de-assertion threshold voltage is 1.63 V.
0x1 [color=#f00]Level 1[/color]: The reset assertion threshold voltage is 2.06 V; the
reset de-assertion threshold voltage is 2.15 V.
0x2 [color=#f00]Level 2[/color]: The reset assertion threshold voltage is 2.35 V; the
reset de-assertion threshold voltage is 2.43 V.
0x3 [color=#f00]Level 3[/color]: The reset assertion threshold voltage is 2.63 V; the
reset de-assertion threshold voltage is 2.71 V.

0 项奖励
回复