Boot uClinux in LPC4357 is impossible?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot uClinux in LPC4357 is impossible?

1,031件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by crchaves on Fri Feb 20 02:59:37 MST 2015
Hi everyone,

Well, I tried to boot the microcontroller LPC4357, exactly in the core Cortex-M4, from several ways but without successful. I know that install uClinux in the Cortex-M4 is nowadays the best OS because have a the good performance, support, facilities ... However, I can't install the OS, the kernel and the FS is ready for my hardware.

If someone that has worked with this processor and has installed uClinux successfully, please Could you help me in the process of booting?

Thanks in advance

Sincerely,

Cristobal 
ラベル(1)
0 件の賞賛
返信
1 返信

987件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Feb 20 10:03:43 MST 2015

Hi Cristobal,
Did you check below thread?
http://www.lpcware.com/content/forum/uclinux-lpc4337-wifibt-device

Also emcraft had ported uClinux on LPC4350. See below link
http://www.emcraft.com/products/232

0 件の賞賛
返信