Boot problem from SPIFI with Hitex LPC1850EVA-A4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot problem from SPIFI with Hitex LPC1850EVA-A4

2,221件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Weizhong-YANG on Tue Jul 09 01:09:21 MST 2013

Hello,


I test an example of LPC18xx.git (LCD_demo)
after programming SPIFI memory if you put the board on,
the program does not work,
you have to press the reset button for the program work?
Anyone knows this problem ?


Wzh

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

2,208件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Aug 23 10:48:03 MST 2013
Hi,
I am glad that you solved the problem.
0 件の賞賛
返信

2,208件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Weizhong-YANG on Fri Aug 23 07:52:11 MST 2013
problem solved, in fact it is the power supply voltage is not correct.
0 件の賞賛
返信

2,208件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Aug 12 21:01:21 MST 2013
Hi Wzh-Y,
Could you please explain the problem again?

Did you have reset and run Checkbox checked on in flash download tab.
0 件の賞賛
返信

2,208件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Weizhong-YANG on Thu Jul 11 00:39:35 MST 2013

yes, in fact the reset button works as a button on / off


I use Keil project,µVision V4.70.0.0
Tool Version Numbers:
Toolchain:        MDK-ARM Professional  Version: 4.70.0.0
Toolchain Path:    C:\Keil\ARM\ARMCC\bin\
C Compiler:         Armcc.Exe       V5.03.0.24
Assembler:          Armasm.Exe       V5.03.0.24
Linker/Locator:     ArmLink.Exe       V5.03.0.24
Librarian:             ArmAr.Exe       V5.03.0.24
Hex Converter:      FromElf.Exe       V5.03.0.24
CPU DLL:               SARMCM3.DLL       V4.70.0.0
Dialog DLL:         DARMP1.DLL       V1.22.0.10
Target DLL:             UL2CM3.DLL       V1.146.0.0
Dialog DLL:         TARMP1.DLL       V1.22.0.10


lpc18xx.git:
2013-03-19 Kevin Wells
<a href="http://sw.lpcware.com/?p=lpc18xx.git;a=summary">http://sw.lpcware.com/?p=lpc18xx.git;a=summary</a>


Thanks in advance,

0 件の賞賛
返信

2,208件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Weizhong-YANG on Thu Jul 11 00:33:34 MST 2013

<span class="hps">yes</span><span>, in fact</span> <span class="hps">the</span> <span class="hps">reset</span> <span class="hps">button works</span> <span class="hps">as a button</span> <span class="hps">on / off</span><span>.</span>


<span>I use Keil project, </span>


<span>µVision V4.70.0.0</span><span></span>


<span>Tool Version Numbers:
Toolchain:        MDK-ARM Professional  Version: 4.70.0.0
Toolchain Path:    C:\Keil\ARM\ARMCC\bin\
C Compiler:         Armcc.Exe       V5.03.0.24
Assembler:          Armasm.Exe       V5.03.0.24
Linker/Locator:     ArmLink.Exe       V5.03.0.24
Librarian:             ArmAr.Exe       V5.03.0.24
Hex Converter:      FromElf.Exe       V5.03.0.24
CPU DLL:               SARMCM3.DLL       V4.70.0.0
Dialog DLL:         DARMP1.DLL       V1.22.0.10
Target DLL:             UL2CM3.DLL       V1.146.0.0
Dialog DLL:         TARMP1.DLL       V1.22.0.10</span>


<span>lpc18xx.git: 2013-03-19 Kevin Wells</span>


<span><a href="http://sw.lpcware.com/?p=lpc18xx.git;a=summary">http://sw.lpcware.com/?p=lpc18xx.git;a=summary</a></span>


<span>Thanks in advance,</span>


 


<span> </span>


<table class="shortlog">
<tbody>
<tr class="dark">
<td title="3 months ago"> </td>
<td class="author"> </td>
</tr>
</tbody>
</table>

 


 


0 件の賞賛
返信

2,208件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Jul 10 22:13:16 MST 2013

Hi,


Do you mean that after programming you turn off the board. You turn it on again and it does not boot. 

0 件の賞賛
返信